This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM5116的最大占空比问题



在TI网站上看到这款芯片的最大占空比是98%,如图

但是打开datasheet,里面有这样一句话,如图

如果强制关断的话也就限制了最大占空比

我输入67V,输出58V的Buck,占空比98%的话我是可以使用这款芯片的,但是如果规定强制关断时间我就没法使用了,不知道这个该怎么理解?