我想问一下 对于我使用LM2678-5.0这个芯片,及经过变压后这个芯片保持恒压5.0V的情况下,输入端的电压从24V到5V,以及16V到5V,两种方案中的发热会差别有多大?
如第一种方案的发热比第二种发热会高很多,还是差别不大? 看到TI的技术说明里面效率是92%,是不是可以理解为发热会差别不大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
会轻微有一些温度差异,比方说输出都是3A, 24V输入时效率86%,占空比是22.8%, 16V输入时效率86.7%,占空比是34%,就功耗而言主要差异在于芯片内部的MOS, Rdson 120ohm, 前者功耗是3*3*22.8%*0.12=0.24w, 后者功耗是3*3*34%*0.12=0.36w, 如果芯片热阻采用T封装45℃/W,芯片温度差异可以估算为45*(0.36-0.24)=5.4℃. (温度差异是5℃左右,以上数据来自TI的webench仿真)