TI辅助设计软件设计出来的电路输出2A,实际测试只能带36V 1.5A,我想做一个输出4A电流的升压电路,能不能直接使用两个MOS并联来获得,电路图有什么需要改的地方?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI辅助设计软件设计出来的电路输出2A,实际测试只能带36V 1.5A,我想做一个输出4A电流的升压电路,能不能直接使用两个MOS并联来获得,电路图有什么需要改的地方?
PCB是按照官方DEMO板画的,理论出2A电流,我带24欧负载的时候输出电压已经是35V左右,已经出现带不动负载的情况,MOS管暂时用的是IRF540,Qg是有点大,内阻也比较高,是不是MOS管的选型导致的上述问题。
还有就是我想问如果我用两个MOS直接并联的方式能不能增加输出电流的能力,查看数据手册LM3478的驱动电流能到1A,驱动两个MOS应该是没有问题。MOS的栅极加了隔离电阻和泄放电阻之后情况还是一样,输出电流大小被限制。
5mΩ的电阻官方给的是0612的,我用的是2512的,功率肯定没有问题。输出电流是不是通过减小Rsense这个采样电阻来实现。
谢谢
HI
我觉得带4A,MOS选取很重要,因为芯片的驱动力可能不够,这点您要确认。(不能选择Qg很大的MOS)
其次注意电感饱和电流一定要足够,按照你的功率36*4/0.85/12*1.2=17A.
HI
因为电流非常大,layout将更加重要,输入电容需要多个并联,并且足够大,尽量靠近芯片Vin和电感的输入端,走线要很宽。
还有就是功率路径。
请问怎么来判定芯片的驱动能力是不是能达到呢,我看手册写的是驱动电流是1A,开关电压范围是0.4-8V,我用示波器查看DR引脚的波形,是700多mV的220KHz左右的开关信号,波形在附件手绘了一个,通过哪个外围器件能改变DR引脚的输出能力
现在选的MOS的Qg是37nC@30V,50A,等效电阻≤7.6mΩ,电感是选用的铁硅铝电感,饱和电流暂时是15A的电流,Layout功率线路的线宽>3.5mm,想先达到3A输出电流,这个选择是否可以
如果将PCB上的功率线路不覆盖绿油直接裸露出来铜皮会有什么影响?
谢谢