使用ucd9244+ucd7242为6678输出四路CVDD,能够正常输出,可是从数字监控端发现电压输出不够平稳,同时设置为1.1V,其实测量的只有1V,最终测试发现PWM调制和7242输出端电感前的波形脉宽波动较大,如图
请问,我该如何调整,使其输出稳定,非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 你这是空载?动态负载还是静态负载时的情况?
2. 通常对于DC_DC开关电源来讲,若是这种输出不同稳定,首先你需要确认你的输入输出电容参数(容值和ESR),电感量选取是否合适(最简单的方法是直接和参考设计进行比对,尽量选参数接近的)
3. Layout布线也会影响和产生这类问题,因此请确认你的UCD7242 驱动的到UCD9244的PWM走线尽量端,而且避开其它的干扰源,VIN脚输入电容也要尽量靠近IC摆放,SW脚到电感的走线也要尽量短,粗,输出电容接地和UCD7242 PGND间走线也尽可能短,粗
4. 若你有分小信号模拟地和功率电源地,这两者之间尽量隔离开
5. 反馈线CSxx,EAxx这些也要避开PWM,电感输入的SW高速干扰线,尽量离远些
1、不是空载,4片DSP里都跑的有一个小程序,第一张图是pwm的输出,第二张是SW的输出。
2、容值参数和我之前另一块板子的一样,这块应该问题不大
3、布线这次的确离得有点远,因为一片控制四路电源,想兼顾,不知道这个影响有多大,再就是EAP和EAN的10欧姆电阻放的靠近9244了。
4、有分9244gnd和GND,用磁珠连接,刚看论坛有人提到这个问题,建议是直接短接,短接后看到没有变化。
5、PWM和FLT在同一层,其他的较远,相邻两层都为地,PWM对线宽有要求吗?PWM线长2700mil
麻烦再给看看
若之前有成功案例,那么参数部分没有问题了,从这个波形也确认可以看出是反馈环路受到了一定干扰,布线的影响比较大些。从9244出来的PWM只是驱动信号,并不直接驱动MOS,因此宽度没有太过要求,10mil 左右也可以,但是长度2700mil有差不多7CM,确实不短。
建议通过飞线,割线的方式尽量建立前面我提到的几点Layout上特别强调的要求试试,看是否会有些改善!