TI专家!您好!我用BQ24170参考评估模板设计了一个双节锂电池充电电路,调试时发现如下几个问题求教。
1、充电电流与设置的值不符
按Icharge=Viset/(20*Rsr) ,Rsr参考官方电路取0.01欧,VREF为3.28V,ISET脚外电阻取值R1为220K,R2为27K,即充电电流约1.8A,没错吧?但实际样板焊接后测试充电时电流却高达2.5A左右,这是什么情况呢?如何解决这个问题?
2、插上电池,上电充电至7.8V左右,绿灯闪烁,充电停止。
在电池电充电至7.8V时,绿灯闪烁,充电停止,从开始充电到出现问题时间大概在1个半小时左右。然后我拔掉电源重新插上,可以恢复正常充电,这是什么情况呀?是充电时间到了,芯片触发保护了吗?如果是充电时间设置过短这个原因的话,那也不对啊,我按Tttc=Cttc*Kttc(Kttc=5.6min/nF) ,取100NF的电容,计算出充电时间为9小时左右。但实际充电1个半小间就触发保护了,这不对哦。是我对芯片资料理解有误,计算方法不对吗?还是其它什么原因呢?求大神赐教,谢谢!
3、不同的电池充电测试,在电池深度放电至0V时,有的可以触发预电模式,有的却不能。
对于这个问题,我的理解是,只要芯片判断电压低于5.7V(实际上所有电池都已经放电至0V)就应该触发预充电,而与电池品牌或厂家无关,因为电池保护板只管放电这块,应该不会干扰到充电芯片的预充电这块,我的理触没错吧?现在我手头的几款电池只有一款可以正常的进行预充电,其它的都不能,按理TI的芯片不会这么挑,我第一次用BQ24170这个芯片,没经验,以上问题请大神多多指点,谢谢!