This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24170充电与电流问题求解!

Other Parts Discussed in Thread: BQ24170

TI专家!您好!我用BQ24170参考评估模板设计了一个双节锂电池充电电路,调试时发现如下几个问题求教。

1、充电电流与设置的值不符

按Icharge=Viset/(20*Rsr) ,Rsr参考官方电路取0.01欧,VREF为3.28V,ISET脚外电阻取值R1为220K,R2为27K,即充电电流约1.8A,没错吧?但实际样板焊接后测试充电时电流却高达2.5A左右,这是什么情况呢?如何解决这个问题?

2、插上电池,上电充电至7.8V左右,绿灯闪烁,充电停止。

在电池电充电至7.8V时,绿灯闪烁,充电停止,从开始充电到出现问题时间大概在1个半小时左右。然后我拔掉电源重新插上,可以恢复正常充电,这是什么情况呀?是充电时间到了,芯片触发保护了吗?如果是充电时间设置过短这个原因的话,那也不对啊,我按Tttc=Cttc*Kttc(Kttc=5.6min/nF) ,取100NF的电容,计算出充电时间为9小时左右。但实际充电1个半小间就触发保护了,这不对哦。是我对芯片资料理解有误,计算方法不对吗?还是其它什么原因呢?求大神赐教,谢谢!

3、不同的电池充电测试,在电池深度放电至0V时,有的可以触发预电模式,有的却不能。

对于这个问题,我的理解是,只要芯片判断电压低于5.7V(实际上所有电池都已经放电至0V)就应该触发预充电,而与电池品牌或厂家无关,因为电池保护板只管放电这块,应该不会干扰到充电芯片的预充电这块,我的理触没错吧?现在我手头的几款电池只有一款可以正常的进行预充电,其它的都不能,按理TI的芯片不会这么挑,我第一次用BQ24170这个芯片,没经验,以上问题请大神多多指点,谢谢!

  • 1. 从你的描述来看,所选电阻R1和R2及最后分得的电压和在Iset上的设定及算法都没有问题,按你这设定确实恒流充电电流是1.8A没错!焊接后不准,帮忙先确认下 a.这个2.5A电流你是怎么测试出来的?  b. 测试ISET脚的电压是否真是0.36V左右?即是刚好是R1,R2电阻分压的结果  c. 确认芯片的焊接和器件都没有问题?没有虚焊,错料,连锡等问题

    2. 先排查问题1, 因为1的不正常已可以说明IC对电流的设定及监测已出现严重失误了,所以截止充电判断也无法保证准确。 从你的描述来看,你是认真研读了规格书的,你的理解没错!计算也合理!

    3. 关于对过放电电池重新充电激活的问题,你的理解合理,但是还是要补充一点。电池深度放电后要能被充电器激活,除了和充电器是否支持0V充电外(显然当前Bq24170是支持的),即与充电器肯定有关系,但是和电池保护板也是有关系的。电池保护板也分支持0V充电和不支持0V充电两类型,所以可能需要具体看看你目前测试的这些电池所带保护板是否有这个差别,判断方法是查看保护板所用保护芯片的规格书

    4. 请问你所用Bq24170 的芯片是从何处获取的?!确保来料质量!

  • 谢谢您的回复!

    对于第1个问题,我采用的是直流稳压电源供电,充电电路的输入电压为9V。ISET脚的电压在没插电池时,测试是0.36V左右,插上电池后,增加到0.58V左右(此时直流稳压电源显示电流约2.5A)。贴片焊接方面我想不会有问题,因为我焊了三片样板,三片都是一样的问题,芯片因为怀疑焊接质量,也有重新焊接过。

    第二个问题,我已经跟电池供应商了解了,他们都说他们的产品可以支持0V充电的,我的芯片样品是采购员从分销商那买的,难道真会是芯片品质本身问题?我在本网站申请样品不成功,提示当前的帐户不能申请样片,不知道是怎么回事?

  • ^_^ 注册了Ti的My Ti账户都是可以申请至少5片免费样片的!若是无效,检查下注册信息是否合适,比如合适的公司信息和公司邮箱。若缺乏一定的公司信息,使用qq,163等非公司邮箱,就要麻烦些!

  • 谢谢,我先申请样品,排除一下芯片品质问题。