This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63001电源管理芯片输出问题

Other Parts Discussed in Thread: TPS63001

我们想用TPS63001做测试,我们想通过EN引脚来控制是否通电,现将测试情况说一下,请帮我解释原因
第一当EN引脚悬空的时候,EN本身引脚上有0.32v的电压,输出端输出为3.3v
第二:当EN引脚直接接地的时候,EN上测出为0v,输出端电压从3.3v衰减到0v,但是衰减速度非常慢,大概10分钟才能衰减到0v
第三,当EN直接接锂电池正极为3.9v电压,输出电压为3.3v。

第四,当处理器的引脚通过100欧姆或者2.2k电阻的时候,TPS63001能正常输出3.3v电压,但是经过2分钟左右,芯片会发热发烫,我电源芯片后面没有接任何电路,当处理器引脚接10k电阻的时候,输出4.5v,我想当处理器引脚3.3v的时候,这个芯片也输出3.3v,请求解决办法
我们想实现的功能是当EN为高电平的时候输出3.3,当EN为低电平的时候,输出为0v。
其中我们的电感选择的是耐电流500ma的0603封装的2.2uh的电感

  • 1. EN脚该IC的推荐做法是有个确定的高或低状态,悬空为不稳定状态,你所测到的0.32V电压是该管脚由IC内部微弱漏电流产生的

    2. EN为0V此时IC被Disable, 所以输出会变到0V,速度很满你需要也同时确认下输出端负载电容是否比较大,导致电池储存的电荷较多,而负载回路阻抗又较大,从而导致放电缓慢所致

    3. 此为IC的正常工作状态。

        你想EN为低时输出迅速放电到0V,若是上面2提到的原因,你可以增加个泄放电路即可,最简单的是比如在输出端接个10K以内电阻到地(当然有MOS开关来控制更好)

  • Hi

       芯片EN脚已经损坏。

       建议按照的电路,测试一下EN脚的电压波形,看是否有很高的电压震荡。

       (我们用处理器控制引脚输出为3.3v(高电平)控制EN引脚的时候,就会烧掉,但是处理器控制引脚加了个100欧姆的限流电阻就可以实现输出为3.3v,加10k的电阻,压降降为1.4v导致不能输出3.3v。En脚漏电流明显大了很多,很可能是EN已经过压损坏)

  • 当按照第一幅图上的原理图实验的时候,当处理器引脚(3.3v)接2.2k或者100欧姆电阻和PEN3连接的时候,能输出3.3v电压,但是经过2分钟左右,芯片会发热发烫,当处理器引脚(3.3v)接接10k电阻和PEN3连接的时候,会输出4.5v电压,请解释一下原因,以及怎么解决
  • 当按照第一幅图上的原理图实验的时候,当处理器引脚(3.3v)接2.2k或者100欧姆电阻和PEN3连接的时候,能输出3.3v电压,但是经过2分钟左右,芯片会发热发烫,当处理器引脚(3.3v)接接10k电阻和PEN3连接的时候,会输出4.5v电压,请解释一下原因,以及怎么解决
  • 应该怎么样设计能保护EN引脚啊?当按照第一幅图上的原理图实验的时候,当处理器引脚(3.3v)接2.2k或者100欧姆电阻和PEN3连接的时候,能输出3.3v电压,但是经过2分钟左右,芯片会发热发烫,当处理器引脚(3.3v)接接10k电阻和PEN3连接的时候,会输出4.5v电压,请解释一下原因,以及怎么解决