我们想用TPS63001做测试,我们想通过EN引脚来控制是否通电,现将测试情况说一下,请帮我解释原因
第一当EN引脚悬空的时候,EN本身引脚上有0.32v的电压,输出端输出为3.3v
第二:当EN引脚直接接地的时候,EN上测出为0v,输出端电压从3.3v衰减到0v,但是衰减速度非常慢,大概10分钟才能衰减到0v
第三,当EN直接接锂电池正极为3.9v电压,输出电压为3.3v。
第四,当处理器的引脚通过100欧姆或者2.2k电阻的时候,TPS63001能正常输出3.3v电压,但是经过2分钟左右,芯片会发热发烫,我电源芯片后面没有接任何电路,当处理器引脚接10k电阻的时候,输出4.5v,我想当处理器引脚3.3v的时候,这个芯片也输出3.3v,请求解决办法
我们想实现的功能是当EN为高电平的时候输出3.3,当EN为低电平的时候,输出为0v。
其中我们的电感选择的是耐电流500ma的0603封装的2.2uh的电感