Other Parts Discussed in Thread: LM46002
打算使用LM46002产生负压,+19V输入,-5.5V输出,负载电流最大1A,看了参考文档,-15V输出时,最小输入电压要求+15V,为什么?我的应用中对输入电压要求是怎样的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM46002
打算使用LM46002产生负压,+19V输入,-5.5V输出,负载电流最大1A,看了参考文档,-15V输出时,最小输入电压要求+15V,为什么?我的应用中对输入电压要求是怎样的?
我的理解是,因为输出负载电流是 电感平均电流和(1-占空比)乘积。 Iout = Iavg*(1-D)。在保证输出1A的情况下,占空比会小于50%。
所以输入大于15V。
可以上BAIDU看看TI关于Inverting buck-boost的应用手册:
http://wenku.baidu.com/link?url=06jP8zC6z8mqXaYynPNbZBKZeCL5YsEI7nZVFBSdiidgpXJv3vRxNvZ0evJeu5g5T7feOMOVlog1KKErd1BuyvAcw7Euhpw9k7oZqXfguWO
谢谢。