在使用TPS5430设计DCDC电路,由24V转6V时发现芯片发热比较异常,稳压源显示24V,电流26MA(负载功率很小),后来测量芯片的PH引脚发现不是方波,请教一下高手这是什么原因造成的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用TPS5430设计DCDC电路,由24V转6V时发现芯片发热比较异常,稳压源显示24V,电流26MA(负载功率很小),后来测量芯片的PH引脚发现不是方波,请教一下高手这是什么原因造成的。
请问一下发烫有多厉害?
由于是在轻载,PH不是方波的原因是因为电路工作在断续模式,由于电路回路纹波电流下降到0,引起二极管和内部MOSFET寄生电感电容谐振。你只要把负载稍微提高,应该能看到谐振消失。
谢谢。
目前只是暖手,比手指温度高一点点,约35度。刚加入约2W的外围模块。波形的确变好了一些,有时候是方波,有时候也是上图的波形。电路输出5V,外围模块耗电大约400MA。测试时电源电压24V,电流115MA左右。外围模块直接使用24V供电时耗电95MA左右。对比起来貌似电路的效率挺高的,但是发热却严重很多,在几分钟内大概到了40度左右,因为需要做其他的测试,所以没有一直通电测试。
如果效率比较高,发热还要看芯片的散热焊盘面积和地的面积大小,还有板子层数。
谢谢。
两层板,散热焊盘尺寸是2.8mm*3.6mm,接地的,散热铜片是裸露在外的,没有加散热片。附近敷铜接地,和手册上一样在散热焊盘上加了4个过孔。目前气温大概30度。
Hi
这个芯片的发热可以借助TI的webench,这个工具很强大,除了可以获得参考电路,以及相关电路参数包括芯片温度,效率等,还可以得到参考layout:http://www.ti.com.cn/product/cn/TPS5430 (在中间右边)