从SwitcherPro里面看到TPS40041这个芯片的最大输出电流为15A,这个15A是由什么来决定的呢?
其限流的电压:Current Limit Threshold是可配的,如果我配置为310mV,我使用的mos管的Rds(on)=3.4mohm,当负载电流达到30A,其侦测电压只有102mV,这个限流也不会起作用吧。
那这个芯片是否就可以输出超过15A的电流呢?
求大神解答??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.