This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40041芯片的最大输出电流问题

Other Parts Discussed in Thread: TPS40041

从SwitcherPro里面看到TPS40041这个芯片的最大输出电流为15A,这个15A是由什么来决定的呢?

其限流的电压:Current Limit Threshold是可配的,如果我配置为310mV,我使用的mos管的Rds(on)=3.4mohm,当负载电流达到30A,其侦测电压只有102mV,这个限流也不会起作用吧。

那这个芯片是否就可以输出超过15A的电流呢?

求大神解答??

  • 你下面的分析是非常正确和合理的!

    理论上TPS40041当然可以输出超过15A的电流,但是现实中需要综合考虑MOS管道过流能力,RDSON,栅极驱动Qg值,TPS40041本身xDRV脚的驱动能力等,所以实际应用中都是有上限的。