This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251-1带负载能力低的问题

Other Parts Discussed in Thread: TPS65251

最近用TPS65251设计了一个电路,BUCK1输出3.3V,BUCK2输出5V。

板子回来后调试发现两路输出的带负载能力都很小,粗略估计不足500MA。

板子是双面板,电感用的是WE的744311470。附件是原理图和PCB的TOP层和BOTTOM层。

说下调试的情况:

1、5V输入时BUCK1输出3.42V,BUCK2输出5.00V,纹波200mV;

2、12V输入是BUCK1输出3.38V,BUCK2输出4.67V,纹波200mV;

3、更换调整开关频率的电阻(390K改成215K)后,不管输入是5V还是12V,两路输出都接近设计值。

TPS65251.rar