This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92510咨询

Other Parts Discussed in Thread: TPS92510, TPS62160, LM3414, TPS92512

最近选择了TPS92510做白光LED(3.2V@1A)的驱动,之前设想是通过PWM调节LED亮度,看到TPS92510是恒流源,而且PWM可以调节线性输出,觉得挺适合。但是实际用了以后发现不能满足使用条件,  如下图,PWM调节后,用CMOS采集LED照明的目标,忽亮忽暗。

我想咨询一下,

1.有没有芯片可以实现PWM对输出电流的完全线性调节,即比如TPS92510,PWM占空比为100%时,VSENSE=200mV,而PWM占空比为50%时,VSENSE=100mV。在PWM调节过程中,输出电压没有变化。

2.TPS92510如图上面标调光方法有PWM和模拟信号两种,我想知道TPS92510如何通过模拟信号调光?如果可行,我可以将PWM信号先通过积分或者DA转换成模拟信号