请教一下,我的5430芯片,看手册上工作电压是5-36都可以用。样板做好后第一次上24V工作电压,与板子连接的芯片全爆了。重新换了板子加12V电压一直工作没有问题,加到18V也没有问题,一上24V就又爆了,对了12V与18V时输出都是5V正常的没有问题。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
芯片上面只剩两根脚的是炸掉的电容吗?
对的,是炸掉的电容。电容耐压是35V的。本来产品正常工作电压是24V,我用的是稳压大功率的电源。我还发现板子上还有一个CAN芯片也烧了,应该是5430输出了一个高于5V许多的电压的电压。其它我还要试一下。
我也比较担心,我买的这个有没有可能是5431改的。如果5431的话会不会在加到24V时5V端会输出一个高的电压。看来电路还得加一个大功率的TVS
谢谢!