This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于5430芯片加电压就爆



请教一下,我的5430芯片,看手册上工作电压是5-36都可以用。样板做好后第一次上24V工作电压,与板子连接的芯片全爆了。重新换了板子加12V电压一直工作没有问题,加到18V也没有问题,一上24V就又爆了,对了12V与18V时输出都是5V正常的没有问题。谢谢!

  • 芯片上面只剩两根脚的是炸掉的电容吗?

    • 用示波器看输入电源是否干净,输入电压慢慢升高,观察输入电压、SW波形,是否有很高的电压尖峰
    • 输入电压升高后,电源效率下降,注意观察温度,看是不是热爆的
    • 周边器件选用要留裕量,不要再爆电容了
    • 芯片来路要严格控制,少量测试可以从TI官网申请样品

  • 看一下输入端电压,是否解耦电容太远,造成尖峰太高,把5430击穿了

  • 对的,是炸掉的电容。电容耐压是35V的。本来产品正常工作电压是24V,我用的是稳压大功率的电源。我还发现板子上还有一个CAN芯片也烧了,应该是5430输出了一个高于5V许多的电压的电压。其它我还要试一下。

    我也比较担心,我买的这个有没有可能是5431改的。如果5431的话会不会在加到24V时5V端会输出一个高的电压。看来电路还得加一个大功率的TVS

    谢谢!

  • 问题应该出在你的输入电源上,你的输入电源如果是那种桌面的试验电源,建议不要直接调整到额定电压上电,因为这种电源有可能在上电瞬间出现一个高的电压尖峰。也就是过充,这就是你在12V级18V输入没问题,而24V输入就损坏的原因,如果你想试验24V输入直接上电是否正常,那建议你在电源输出到你的板子之间加一个开关,先打开电源,等电源输出24V稳定后,闭合这个开关,这样可以保证输入不会出现高的电压尖峰,你可以试试,这种情况我经常遇到。

  • 感谢提醒,我会注意的。电源是80V 30A智能恒流电源,连接到电路板有安装有空气开关。