This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:sbs0x08读的是哪个传感器的温度?



昨天发了一贴,可能问题太多了,没人回答我。www.deyisupport.com/.../115091.aspx

今天请教得简单一些。

sbs命令0x08读的是TS1还是TS2,还是内部传感器的温度?

  • The source of the measured temperature is configured by the [TEMP1], [TEMP0] bits in the Operation Cfg A register.

    TEMP1, TEMP0— These bits configure the source of the Temperature function.

    0,0 = Internal Temperature Sensor

    0,1 = TS1 Input (default)

    1,0 = TS2 Input

    1,1 = Average of TS1 and TS2 Inputs Related Variable: SBS:Temperature(0x08)

    可i配置。