昨天发了一贴,可能问题太多了,没人回答我。www.deyisupport.com/.../115091.aspx
今天请教得简单一些。
sbs命令0x08读的是TS1还是TS2,还是内部传感器的温度?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
昨天发了一贴,可能问题太多了,没人回答我。www.deyisupport.com/.../115091.aspx
今天请教得简单一些。
sbs命令0x08读的是TS1还是TS2,还是内部传感器的温度?
The source of the measured temperature is configured by the [TEMP1], [TEMP0] bits in the Operation Cfg A register.
TEMP1, TEMP0— These bits configure the source of the Temperature function.
0,0 = Internal Temperature Sensor
0,1 = TS1 Input (default)
1,0 = TS2 Input
1,1 = Average of TS1 and TS2 Inputs Related Variable: SBS:Temperature(0x08)
可i配置。