This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54561技术问题

Other Parts Discussed in Thread: TPS54561

我们在测试TPS54561时遇到以下问题,请指教,谢谢!

1.试TPS54561白盒应力IC Fa‘il(SS脚应力测试波形有周期性的尖峰,满载明显大于空载。尖峰值大于SS的最大规格值(datasheet标注最大值3V)。)还请帮忙分析下原因和风险,目前是3.2V,客户想知道会不会有问题,要给终端客户答复。

a.输入8VDC,输出5V2A

b.输入36VDC,输出5V2A

2.目前此项目在调试过程中发现,输出下电开始的时候有一次振荡,下电完成后输出还有重启的迹象:

a. 输出下电开始的时候有很大的几率有一次振荡,目前改动boot-sw电容 C303到0.33uF有一定效果,但是高温85℃测试还是有一定几率出现,请帮忙看下什么原因,继续加大C303会不会有其他隐患

b. 下电完成后输出还有重启的迹象,目前加大假负载R263=560Ω,有改善,能否帮忙看看是什么原因。

tps54561测试波形.docx