下面是原理图,我为了测试TPS40200限流保护部分的电阻的效果,每个电阻都并联一个0欧电阻用于短接。
下面是实际的Layout,敷铜去掉后的3D图,比较清晰
R3我实际接的是65m的合金电阻。
现象如下(42V输入,12V输出):
1、当没有R3的时候,电流可以很大(实际测试时到1A就没继续测试了,因为R4温度比较高怕烧坏)
2、当没有R4和R5的时候,当电流上升到1.1A时,输出就截止了
3、当没有R4、R5、R1时,上电就截止,电流多小都不行
4、当没有R4、R5、R1、R9时,电流达到1.7A时输出就截止了
5、当没有R4、R5、R1、R9、R6时,电流达到1.2A时输出就截止了
所以呀很奇怪,按手册VDD和ISNS的压差达到100mV限流保护才会起作用,输出截止。