This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24600的ACDRV电路的用处?

Other Parts Discussed in Thread: BQ24600EVM

1、请问在BQ24600EVM的线路板中,需要将ACDRV到ACDRV_IN短接,请问短接的作用是什么?
2、为什么不短接时P\G\脚位呈现高电压,是由于什么原因引起的?
3、我ACDRV到ACDRV_IN不短接,直接在AB两处加供电电压,为什么没有正常工作?
多谢!
  • E2E上已解答:

    The  circuit in the red box, along with the FET connected to the BATDRV circuit  in the evm, gives the bq24600 functionality similar to the other  devices  in  the  600 family. It  allows the IC to "select" where  system power is coming  from (battery or adapter).

    Replacing  them  with  a diode  is perfectly acceptable.