文档里说this is the most time-consuming option
根据经验,这个大约用几个小时呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你说的是chenistry ID选择以后需要做一个完整的电芯学习过程。
整个过程参考如下, 时间大概要14h左右。
A、确认已经设置好相关的参数以及进行校准和CHEM_ID选择才可以进行此步骤,发送命令0x41复位,导出DFI文件或者SENC文件备用
B、准备好一个放空的电芯(电压在3.0V-3.3V),静置5小时
C、连接板,发送0x0021命令使能IT算法,建议自动记录Data RAM数据(4s间隔)Data FLash数据(10分钟间隔)
D、按照正常充电过程将电池充饱,然后静置2小时,再按照0.2C电流进行放电到截止电压,再静置5小时,确保update status的数值为0x06
E、导出DataFlash的gg文件,用记事本打开修改Update Status为0x02,Cycle Count为0
F、导入之前备份的DFI或者senc文件,然后再写入修改后的gg文件
G、生成DFI,dffs文件
可以参考Achieving The Successful Learning Cycle 地址如下:http://www.ti.com.cn/cn/lit/an/slua597/slua597.pdf