This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ14201H模块纹波问题



小白参照simple switcher系列的LMZ14201H的Datasheet设计了设计了24V输入、15V(2.5A)、5V(1A)-15V(1A)的电路,电路原理图如下:

并参照了Datasheet后面的PCB布板,画出了最终的PCB,如下:

分别测试了电源空载、带60%负载时的输出电压纹波(测试纹波时,探头没有加电容,但是尽量保证地线最短),发现纹波比较大并且波形也不大对。现在不知道具体哪里出了问题,希望大家能给我指点一下,让我有个思路,非常感谢。

空载波形

60%负载波形