This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

太阳能充电控制器解决方案SM72295

Other Parts Discussed in Thread: SM72295, SM72442

您好。

TI的解决方案SM72442和SM72295 的组合 请问下,最大可以支持多少功率,对应的怎么配置.

  • 您好,

    请问您的应用是什么?太阳能充电器?需要的输入电压、最大输入电流、输出电压和最大输出电流是多少?

    目前有SolarMagic™ SM3320-BATT-EV 充电控制器参考设计http://www.ti.com.cn/tool/cn/sm3320-batt-ev,适用于12V Lead Acid Battery充电,输入电压Vin range = 15V to 45V Vmp (50V Voc),最大输入电流Max Input Current: Isc = 11A。可参考。

  • 您好!我刚刚购买TI的SM3320-BATT-EV参考设计样机进行调试,该样机是12V电池充电设计。我按照设计书的规格搭建了实验平台,但是样机无法工作。请问是什么问题?

    1.参考设计中,SM72442 A0管脚接的电阻分压支路,5V电源接的电阻被取掉了,请问我需要重新计算并自行焊接一个电阻吗?还是说,样机不需要任何处理直接接入电池板和负载就可以工作?

    2.样机P1 接口需要接上吗?那个应该是做通讯用的,我想知道是否接地会不会影响工作