您好。
TI的解决方案SM72442和SM72295 的组合 请问下,最大可以支持多少功率,对应的怎么配置.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请问您的应用是什么?太阳能充电器?需要的输入电压、最大输入电流、输出电压和最大输出电流是多少?
目前有SolarMagic™ SM3320-BATT-EV 充电控制器参考设计http://www.ti.com.cn/tool/cn/sm3320-batt-ev,适用于12V Lead Acid Battery充电,输入电压Vin range = 15V to 45V Vmp (50V Voc),最大输入电流Max Input Current: Isc = 11A。可参考。