Other Parts Discussed in Thread: MSP430FE427
有谁用过ADE7763这款芯片吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADE7763是一款高精度,支持IEC 61036 / 60687,iec62053-21,和iec62053-22on-chip数字积分器,在当前通道允许直接接口分流和电流互感器有功能量、波形和明显的电流传感器,在25°C正能量积累模式对芯片的用户可编程阈值电压凹陷和程序储存校验标定功率、电流和电压的相位和最少有效值比有功电能计量的动态范围超过1000误差0.1%,1,和输入芯片温度传感器(±3°C典型)的补偿、SPI®-可编程频率中断请求引脚兼容的串行接口脉冲输出(IRQ),5 V电源供电,低功耗(25 mW典型
MSP430FE427是TI自带计量的CPU,32K的FLASH和1KRAM内存,满足一般计量要求。
您好! 你有ADE7763的相关代码吗? 我现在想用模拟的spi进行移植。
抱歉哦没有相关的代码,上个回复附件里面有这个芯片的工作原理,请参考即可