1、CD4051应用在小信号放大器上
2、8路选择开关,调整放大器倍数,用来调整灵敏度。
3、运放正常状态下,没有小信号输入的时候,输出是3V,运放输出双限位,Hv=4V,Lv=2V
4、我测试架设置输出2.9-3.1为正常偏差
5、装上CD4051时,输出出异常,没有小信号时,输出是3.0-5V这个区间的都有,不良率接近50%
6、怀疑是CD4051的漏电流大造成的,测试运放输出3.5V与4V的两个IC的漏电流,分别为10nA与82nA
7、测试CD4051的通道能够正常切换,但是切换通道,没有小信号输入时,运放输出有时会变化
8、到底是不是CD4051通道的漏电流造成的呢?求分析?
9、电路上有改进措施么?CD4051有漏电流小的替换物料么?
10、附件是电路图