This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4051应用在放大器上,运放输出异常。生产1000,不良456,返工费用高,急急急!!!


1、CD4051应用在小信号放大器上

2、8路选择开关,调整放大器倍数,用来调整灵敏度。

3、运放正常状态下,没有小信号输入的时候,输出是3V,运放输出双限位,Hv=4V,Lv=2V

4、我测试架设置输出2.9-3.1为正常偏差

5、装上CD4051时,输出出异常,没有小信号时,输出是3.0-5V这个区间的都有,不良率接近50%

6、怀疑是CD4051的漏电流大造成的,测试运放输出3.5V与4V的两个IC的漏电流,分别为10nA与82nA

7、测试CD4051的通道能够正常切换,但是切换通道,没有小信号输入时,运放输出有时会变化

8、到底是不是CD4051通道的漏电流造成的呢?求分析?

9、电路上有改进措施么?CD4051有漏电流小的替换物料么?

10、附件是电路图

RS-SC20-V01.pdf