This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202 的EN脚疑问

Other Parts Discussed in Thread: TPS54202

你好!

客户使用TPS54202,输入电压12V,输出3.3V/2A,现使用的是上电直接使能的方式。

在原理图设计时由于疏忽,将EN脚通过100K上拉电阻直接接到12V的输入电压轨,现通电可以输出3.3V。

后经查询规格书,确认EN引脚的输入电压最大不能超过7V,我有测量EN脚,这时候的电压时6.8V。

请问EN脚的6.8V是如何产生?

长期使用的话可能会导致什么问题?谢谢!