This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助TPS43061 无法升压,VIN和EN电压正常,输出比输入低

原理图如下

其中R57,R58用了12欧电阻代替,R55和R56两个检测电阻先都用了10毫欧的,后改成一个10毫欧的,电感最先用了6.8uH的一体成型电感,后换为15uh的功率电感,输出不变,输入电压25.6V,输出为25V,根据查阅手册,芯片应该是处于未工作状态,量了各管脚电压如下:

  1. RT/CLK:0.5V
  2. SS:3.2V
  3. COMP:2.12V
  4. FB:1.13V
  5. ISNS-:25.6V
  6. ISNS+:25.5V
  7. VIN:25.5V
  8. LDRV:0
  9. PGND:0
  10. VCC:5.4V
  11. BOOT:25.1V
  12. SW:25.5V
  13. HDRV:25.1V
  14. PGOOD:5.3V
  15. EN:3.0V
  16. AGND:0

根据手册,VIN>4.5V,EN>1.21V,芯片应该工作,但是输出出现跟随输入现象,PGOOD为高,PCB也是按照手册进行的布局和布线

请各位大神帮忙看看,到底是哪里的问题,不胜感激