This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195充电电流有问题,无法大电流,有时候电流还很小?

REG00设置0x35或0x37,REG08读到0xAC,REG09为0x00。

用华为5V/2A的适配器,最大电流1A多点,不超过1.5A,没有达到默认设置的2A。

有时候电流会很小,200毫安左右,处于快充阶段,这个问题最困扰。

适配器电压会下降到4.5V左右。

把REG00的输入电压限制设置低点,电流会变大,但是有时会充电出错。

是用USB检测仪测的电流,并根据适配器发热程度判断电流。