REG00设置0x35或0x37,REG08读到0xAC,REG09为0x00。
用华为5V/2A的适配器,最大电流1A多点,不超过1.5A,没有达到默认设置的2A。
有时候电流会很小,200毫安左右,处于快充阶段,这个问题最困扰。
适配器电压会下降到4.5V左右。
把REG00的输入电压限制设置低点,电流会变大,但是有时会充电出错。
是用USB检测仪测的电流,并根据适配器发热程度判断电流。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
适配器电流太小了,请保证输入电压不会低于设定的dpm电压,将看门狗关闭,输入电流,充电电流设大,外部限流电阻设小或者禁用,电池电压保持在3.9V,在这种情况下如果电流还是上不去,那就是PCB和电感的问题。
你这个描述来看,明显是USB接口的问题,要么就是D+/D-接触不良,要么就是Vbus或GND接触电阻太大,引起线路上压降太大,手机端输入电压低,手机判断为适配器过载启动了VIN DPM(动态管理)。
输入限流设置为3A也是没问题的,只是如果充电电流也很大的话,适配器的电压会被拉低很多,有些时候是不允许的。
建议还是通过适配器类型来选择输入限流。