This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610状态指示灯的问题



经典原理图做的4节串联18650电池充电器,充放电的电压和电流都正常,我用EV2300读的电池数据。就是STAT1 和 STAT2 的状态指示灯不对。 没接电池时: STAT1的灯闪烁,STAT2 灯不亮。 接上电池时:STAT1的灯常亮,在充电,电流与设置的参数一致,1A电流;充电电流减少到20mA时,电池已充满电,电池设置电流低于20mA截止充电,这时候STAT1的灯变成闪烁,STAT2的灯不亮,而不是规格书说的STAT1灯灭,STAT2灯亮。

充满电时,VFB的电压在2.1V。

请问这是什么情况?

PS:原理图上面的地都是同一个地。

锂电池充电器V1.pdf