使用BQ24113A对两节锂电池充电,Rsns=0.1Ω,Riset1=Riset2=10K。
充电电流1A,减小到0.1A充电停止。
测试中发现充电至8.4V、充电电流小于0.1A并没有停止。在低到30mA左右时,仍在充电。
请问这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢你的反馈,按照目前的情况,建议你对比我们evm的layout检查一下(见如下链接中的page 10)sense电阻到SNS和BATpin 之间的trace,这个sense电阻应该尽量靠近芯片,需要注意的是SNS/bat引脚应该尽量直接接到R4两端上,之间的trace一定不能太长。不要把电感和sense电阻之间的trace夹带到SNS和BAT之间了(这样会引入大量的线阻和寄生感抗),此外尽量不要在sense电阻旁边打过孔或有并行的大电流trace。