This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24113A充电停止条件问题

Other Parts Discussed in Thread: BQ24113A, BQ24103A

使用BQ24113A对两节锂电池充电,Rsns=0.1Ω,Riset1=Riset2=10K。

充电电流1A,减小到0.1A充电停止。

测试中发现充电至8.4V、充电电流小于0.1A并没有停止。在低到30mA左右时,仍在充电。

请问这是什么原因?

  • 根据你描述的现象,我有一些担心你是否实际使用的芯片是BQ24103A,因为它有一个TTC pin(7脚),如果这个脚被拉低,那么小电流截止检测功能会被禁止从而出现你描述的这个现象,因此你可以用一个0.1uf的电容接在第7pin上看看是否由这个原因引起的问题。

  • cheng,

       如果确实是使用BQ24113A,当电波低到30mA时,这么小的电流测量可能会有误差,请确实测量得的电流为真实值。STAT1及STAT2各是什么状态?另外RSNS的电阻精度对充电状态也会有影响,建议使用高精度的检测电阻。

  • to  Michael Yang

        丝印CKF,确认是BQ24113A。CMODE端通过10K电阻上拉到Vtsb。

    to  Trevor

        1.Riset1与Riset2选用同样电阻,充电电流为1A,应该可以间接说明不是Rsns电阻精度问题。

        2.用了两块电路板,万用表用不同电流档测量,均有同样问题,基本可以排除个别芯片问题或万用表准确度问题。

        3.STAT1一直是ON的状态。显示充电中。STAT2在BQ24113A上不存在。

  • 感谢你的反馈,按照目前的情况,建议你对比我们evm的layout检查一下(见如下链接中的page 10)sense电阻到SNS和BATpin 之间的trace,这个sense电阻应该尽量靠近芯片,需要注意的是SNS/bat引脚应该尽量直接接到R4两端上,之间的trace一定不能太长。不要把电感和sense电阻之间的trace夹带到SNS和BAT之间了(这样会引入大量的线阻和寄生感抗),此外尽量不要在sense电阻旁边打过孔或有并行的大电流trace。

    www.ti.com.cn/.../sluu200a.pdf