如上图,用TPS51220产生两路电压:12V和5V,输入电源为19V。因为环境原因,电源输入端偶尔有电压暂降(跌落)的情况,这个时候12V没有输出,在电压稳定时,不能自启动,但是用镊子短接控制端EN2再放开,12V又出来了。如果12V输出改为3.3V或5V输出,输入电源端(Vin)随怎么波动,电压稳定时,IC都可以自启动,正常输出。
电源输入暂降跌落这种情况,要怎么调哪里的参数,才能让12V自启动正常输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
看起来您输入电压在启动瞬态转换时跌落得比较厉害,因为这款芯片支持接近100%duty转换。
建议你在输入增加100uF电容用于稳压。在layout上输入电容需要尽量靠近MOS输入端,MOS与电感尽量紧凑点。
Hi
增加稳压电容只对瞬间的电压跌落有稳压作用,持续的跌落是没有效果的。
或者这个问题只能从源头解决,因为很可能在较低电压启动时,12V输出会触发欠压保护,这个是需要重新Enable才能正常输出的。建议你按照实际应用条件(不要模拟),测试12V的波形做确认。
如果源头无法解决,可以考虑增加一个自动的电路。(确认后我将提供给你)
实际应用基本情况就是:市电有波动,适配器输出19V有掉电,导致12V输出掉电,等市电回稳时,19V稳定了,但是12V没有启动正常输出。市电端是有大功率设备启动,加上19V电源适配器质量差,大功率设备启动完成后那个时间点正好是12V已经掉到低了。
如你分析那样低压启动触发了12V欠压保护,必须在EN2端重新启动。我做了一个掉电检测,比较器+几个阻容,比较输出到EN2端泄放电,等来电断开泄放回路时则重新启动。但是这些料件在后面的改版上空间受限,估计都摆不上。还希望你提供自动电路参考。
现在头疼的是,现场的几百片成品不知道怎么处理,如果基于图纸改几个物料的参数能调好就最好了!!
Hi
如果EN2脚没有电容,而EN电压跌落时间不够说明外部大功率系统启动时间其实还是很快的(输入电压有跌落但是跌落后上升也很快)
可以做2个试验:
1. 将之前电路设置的13V改到17V,这样可以更快的拉掉EN(修改上面一个电阻)
2. 在输入并联2~3个2200uF电容,延缓跌落(之前建议的100uF可能太小了)
HI
周末想了一下,EN2加电容比不加电容好,因为三极管放电很快,你可以将门槛值设置到18V。而充电是通过上拉电阻,你也可以将上拉电阻加大一点,这样快放慢充,是可以完成reable的。