This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

charger management

Other Parts Discussed in Thread: BQ24773

关于BQ24773,请问是否有Demo Kit及MTK/Linux平台下的驱动支持?

还有一个问题,多节串联电池的充电IC和单节高电压的充电IC有什么区别吗?

举个例子:比如(BQ24261M)

  • 我们没有这方面驱动程序的支持哈,多串电池的电压比较高,比如3串电压最高为12.6V或者更高,而单串的输出最大电压是4.2V或者4.35V。如果都用来设计单串电池充电器,那么单串的IC价格会低一些。

  • 您好,我们的需求是有3节电池一起使用(因为尺寸限制,单节的容量较小)。又因为平台是手机平台,所以需要的输出电压和普通单块电池一致4.2V/4.35V

    请帮忙参看一下是并联还是串联比较合适?并且,选中什么样的IC合适?谢谢您

  • 这个要权衡了,如果系统里面都市低压应用,那么采用并联,单节电压输出,那么电源转换效率会比较高,但是电池可能无法放到最低的3.0V左右,一般需要在3.4V左右截止,对于充电也只需要单节充电芯片,如果还有高压需求,串联起来都采用buck结构,电路设计较简单,同时电池也可以放到3.0V最低。但是充电芯片需要支持多节充电,如果输入电压较低,那么还需要boost充电,那么就比较麻烦了。

  • 您好,我请问下,就是这两种情况下,TI是否有合适的IC可以推荐吗?非常感谢