关于BQ24773,请问是否有Demo Kit及MTK/Linux平台下的驱动支持?
还有一个问题,多节串联电池的充电IC和单节高电压的充电IC有什么区别吗?
举个例子:比如(BQ24261M)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们没有这方面驱动程序的支持哈,多串电池的电压比较高,比如3串电压最高为12.6V或者更高,而单串的输出最大电压是4.2V或者4.35V。如果都用来设计单串电池充电器,那么单串的IC价格会低一些。
这个要权衡了,如果系统里面都市低压应用,那么采用并联,单节电压输出,那么电源转换效率会比较高,但是电池可能无法放到最低的3.0V左右,一般需要在3.4V左右截止,对于充电也只需要单节充电芯片,如果还有高压需求,串联起来都采用buck结构,电路设计较简单,同时电池也可以放到3.0V最低。但是充电芯片需要支持多节充电,如果输入电压较低,那么还需要boost充电,那么就比较麻烦了。