This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24170充电指示间接性闪烁

Other Parts Discussed in Thread: BQ24170

TI:

我用的BQ24170给两节串联的锂电池充电,我的电路跟datasheet首页的Typical Application Schematic略有不同:

1.AVCC端我只用Adapter供电,没有加那两个二极管接到VBAT上

2.SW引脚上的二极管也没有接

3.BATDRV 接的 PMOS用的SI2305  低压差的PMOS

4.系统整个负载我是直接加在电池的两端的,而不是像典型应用的通过Q3进行选择的

现在问题是我刚插上电池的时候能充电,2-3秒后指示灯开始闪烁,我用示波器测量SW引脚,发现是一会有PWM,一会没有。我觉得是刚开始充电,然后就保护停止了,然后再开始,往复循环。插图为我的电路原理图及PCB,请大神看看问题出在哪?

  • 按照datasheet上的检查顺序都测了没问题,这就奇怪了,我的直流电源是12V

  • 两个问题先澄清一下

    1.上电顺序。建议顺序是,先插电池,再插适配器。

    2. 负载电流多大?有没有可能负载电流太大了?把负载先去掉看看什么结果?

  • 1.上电顺序没问题,确实是先插的电池,然后才插适配器

    2.现在我单独焊接了一块没有任何负载的电路,应该也不是负载的问题

    question2:我的原理图跟EVM的差别如上列举的几个,不会是电路有问题吧?

    question1:现在我的TTC引脚是接的0.1uF的电容,当我把TTC引脚短接到地的时候充电指示灯正常了,但是电池的充电引脚一直维持在8.4V左右,单独测电池电压7.6V,这个应该是不正常的吧,我用示波器观察SW引脚确实是连续的PWM信号。这样是说明已经正常充电了吗?附图是datasheet中TTC的说明