This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117问题请教



电路原理图和手册典型电路一样,空载的时候输出都对。但是加0.5A负载的时候,芯片就进入了Hiccup Mode,起初怀疑是采样电阻干扰太大,后来就直接断开采样电阻,在芯片管脚就近用0Ω电阻把CS和CSG短接,只把CSG连接到采样电阻,但是即使这样,带0.5A负载时,芯片还是进入了Hiccup Mode。特来宝地,请大神答疑解惑。谢谢!

  • Hi

       即便将电阻设置为0欧姆,是否有用示波器直接测试CS脚波形?

       这里的电阻本身就非常小,即便0欧姆,仍然是有阻值的,而其noise远远大于其Rs产生的电压,同时10倍放大。

       可能你的layout不是特别好才导致的过电流误保护,建议你在CS脚增加滤波器,2个100ohm+1nF, 电容尽量靠近芯片CS脚。

      (可以先加电容测试看看)

  • 电容有加470p,没有效果,我才直接拿0欧姆电阻短接的,那我试试把电容加大再看看。

  • Hi

        470pF没有效果,1nf也悬, 直接用示波器测试能有发现吗?

        (可能功率路径和GND没有layout好)

  • 不是470n是470p,直接用示波器看,看到的全是开关尖峰。layout肯定是不好,我再想能不能先手动调整一下,看看哪些是关键因素,能正常工作了,再有针对性的改板。

  • Hi Johnsin,

    我尝试将RAMP脚直接0欧姆短接到地,CS和CSG也同时短接到地,目前可以带负载了。但是我发现另外一个问题,在这种情况下,输出电感电流总是不能连续,开关频率也会随着输入电压升高而下降。针对这个问题,你能帮我解答一下么?下图中,蓝色是半桥输出电压,紫色是输出电感电流。

  • 开关频率的问题如下所述,条件:输出12V电流2A

    输入为25V时,上管的驱动波形

    输入为30V时上管的驱动波形

    输入为35V时上管的驱动波形:

    从上可以看出开关频率随着输入电压一直在改变。我反复确认了RT脚的下拉电阻为22k,理论上开关频率应该在220kHz左右,但是实际差别好大。请问一下芯片内部会自己调整开关频率么?还是有其他原因。

  • Hi

       建议重新layout后测试确认。

       在没有CS侦测的情况下都电流保护,ramp脚都因为noise影响到了,芯片很难正常工作。