This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3895

Other Parts Discussed in Thread: UCC3895

TI专家们好!

学习了移相全桥一段时间,最近利用UCC3895搭建了一个电路,在调试过程有一些疑问,希望能得到专家们的解答。

1、UCC3895的控制方式有电压控制、平均电流控制和峰值电流控制,但是目前没有看到过电压控制的外围电路,不知道是什么样子的。

2、UCC3895一般都选择峰值电流控制,峰值电流控制就涉及到斜坡补偿的问题,我看了相关的资料,基本上都是在3脚RAMP和7脚CT之间接一个三极管,这个三极管是如何起到补偿作用的。

3、调试的时候问了一些前辈,有人建议我先不管补偿,直接将7脚CT接到3脚RAMP上,不知道这样是否可行。如果可行,那么3脚RAMP的对地电容就要拿掉了,否则会影响到锯齿波的频率。峰值电流控制,CS脚的电压是否可以不引到3脚RAMP上。

4、UCC3895内部电压误差放大器接成跟随器的形式,20脚EAP与3脚的RAMP比较生成PWM,这里想问一下20脚的电压范围是不是要限定在1V~3.6V的范围(考虑RAMP脚内部有一个0.8V的偏置)。如果EAP电压低于1V或者高于3.6V会出现什么问题?

下面是我设计的芯片外围电路和电压反馈电路,请帮忙参详一下是否有问题。

谢谢!

  • 1、电压型控制就是在RAMP端引入固定的三角波,误差放大器输出跟固定三角波比较调整占空比的。

    2、斜坡补偿不仅仅是加一个三极管,而是用CT控制三极管产生一个三角波,然后通过一个电阻接到RAMP端,你看看,肯定存在这个电阻的。

    3、给你这样建议的人,就是让你做成电压型控制模式。

    4、不用人为控制,环路会自动调整。

  • 首先感谢您的回答!

    根据您的回答,我想请教以下几个问题:

    1、三极管的输出确实接了一个电阻到RAMP,那么这个电阻的组织一般如何取。还有如果加了一个三极管就会造成3895在占空比较小时有跳跃现象,这该如何解决。我尝试了在CT和REF端加电阻提高晶体管的基极偏置电压,但是电阻的数量级不好控制。

    2、ADS和CS脚有2个电阻用来控制自适应死区时间范围的,这两个电阻的阻值一般取什么数量级的?

  • 1、三极管接的电阻与电流信号接到RAMP端的电阻,共同形成斜坡补偿,具体要看你补偿的幅度是多少来选择。

    2、具体的应用你可以看看PDF文档,因为这个IC我没具体用过,所以不太清楚该如何计算。