BQ34Z100g1使用的是7002 MOS进行分压,稳压的LOD,我现在做到13-15串高电压的电池组,发现电压在50多V的时候,7002摸上去持续几秒会发烫,空载实测整个板的耗电已经到达毫安级别了,我的15串保护模块耗电比较低,几十uA级别,几乎可以忽略不计。 请问这正常吗?(此时我已经取下74HC164这个逻辑IC了,光BQ34Z100G1+7002这个电路耗电到了mA级别,我不能接受)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ34Z100g1使用的是7002 MOS进行分压,稳压的LOD,我现在做到13-15串高电压的电池组,发现电压在50多V的时候,7002摸上去持续几秒会发烫,空载实测整个板的耗电已经到达毫安级别了,我的15串保护模块耗电比较低,几十uA级别,几乎可以忽略不计。 请问这正常吗?(此时我已经取下74HC164这个逻辑IC了,光BQ34Z100G1+7002这个电路耗电到了mA级别,我不能接受)
你好 我还有一个问题就是如何将bq34z100-g1 进入低功耗模式也就是深度睡眠模式,我写了代码但是不知道怎么回事就是进不去,求大神帮忙。
void sendmsg_to_bq34z100(uchar command,uchar data1,uchar data2)
{
iic_start();
iic_send_byte(0xaa); // Address
iic_receive_ack(channel);
iic_send_byte(command); // Gauge command
iic_receive_ack();
iic_send_byte(data1); // Data: low byte
iic_receive_ack();
iic_send_byte(data2); // Data: high byte
iic_receive_ack();
iic_stop();
}
sendmsg_to_bq34z100(0x01,0x10,0x00);
以上是进入休眠的代码 但是不知道什么原因 不能进入休眠,而且已经确定iic通信没问题。