BQ24195, 输入USB 5V,具体测量为4.67V. 系统从SYS端口取电,但是发现在不接电池的情况下,SYS每200ms会有一个大概2V左右的电压跌落。ILIM如下图,测量ILIM引脚得出最大电流仅为340mA。输入部分没有明显电压跌落。所以这是和电池检测相关的正常现象还是芯片/设计问题?
(D+ D-悬空)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ24195, 输入USB 5V,具体测量为4.67V. 系统从SYS端口取电,但是发现在不接电池的情况下,SYS每200ms会有一个大概2V左右的电压跌落。ILIM如下图,测量ILIM引脚得出最大电流仅为340mA。输入部分没有明显电压跌落。所以这是和电池检测相关的正常现象还是芯片/设计问题?
(D+ D-悬空)
Hi
可以不要电池,正常不应该有电压跌落。
建议你确认一下USB供电电流限制,是否满足系统SYS的电流需求? (或者你将负载减小,看不良现象是否消失?)