This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195在不接电池的情况下,SYS有间隔性电压跌落,是否正常?

Other Parts Discussed in Thread: BQ24195

BQ24195, 输入USB 5V,具体测量为4.67V. 系统从SYS端口取电,但是发现在不接电池的情况下,SYS每200ms会有一个大概2V左右的电压跌落。ILIM如下图,测量ILIM引脚得出最大电流仅为340mA。输入部分没有明显电压跌落。所以这是和电池检测相关的正常现象还是芯片/设计问题?

(D+ D-悬空)

  • Hi

       可以不要电池,正常不应该有电压跌落。

       建议你确认一下USB供电电流限制,是否满足系统SYS的电流需求? (或者你将负载减小,看不良现象是否消失?)

  • 输入断没有电压跌落,输出端电压跌路如图。输入有2A保险,供电为电脑,而且测量没有跌落。负载的话,我们发现在打开ESP32芯片的DCDC的时候会产生如图的电压跌落,但是如果街上电池,该现象就会消失。是否是芯片设置问题?

    而且必须是先上电,再插电池。如果直接插电池,输出电压异常。

    (以上测量都是在SYS端)