This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25895充电问题

Other Parts Discussed in Thread: BQ25895

有几个问题请教下

1.规格书上说,bq25895最大充电电流可以到5A, 这有没有特定的输入电压要求。我在外部稳压源输入10V以上时可以达到5A的充电电流,但输入电压为5V时,达不到5A

2.如何让快充输出不同的电流,我买了华为的充电器SuperCharge 支持5V/2A,4.5V/5A,5V/4.5A ,但使用时只能输出5V/2A,是否895不支持这个充电器

3.用外部稳压源输入,当逐渐调低电压的时候,895会停止充电。电压升高没事。

  • Hi

           输入的限流电是3.25A,  而topy上是降压,电池充电是5A时,假设此时buck的输出是4V, 效率是90%,输入电流为3A,   那么4V*5A/90%/3=7.4V,  所以并非所有电压范围内都能维持5A充电。如果你的效率达不到,并且电池电压较高导致buck输出较高,则需要更高的输入电压。

          如上,当输入电压较低时,电池充电电流也就较小了。在可充电范围内电流可通过寄存器设置。

  • 那还有一个问题,在不接外部电源的时候, PMID输出5.1V,接了外部电源,PMID会电压升高到输入电压,是否在充电的时候,PMID就不能用了。 如果要做个产品 在充电时,也能对后5V放点,要不要另加电源管理芯片?

  • Hi

       是的,充电的时候是用buck电路。 PMID是在不充电时boost电路, 两个是同一个电路,所以不能同时出现2种功能。

  • 另外BQ25895支持的快充协议,是不是针对高通的,因为我用小米的快充可以正常检测到,并输出12v1.5a,但用华为的快充,只能识别到5v2a