有几个问题请教下
1.规格书上说,bq25895最大充电电流可以到5A, 这有没有特定的输入电压要求。我在外部稳压源输入10V以上时可以达到5A的充电电流,但输入电压为5V时,达不到5A
2.如何让快充输出不同的电流,我买了华为的充电器SuperCharge 支持5V/2A,4.5V/5A,5V/4.5A ,但使用时只能输出5V/2A,是否895不支持这个充电器
3.用外部稳压源输入,当逐渐调低电压的时候,895会停止充电。电压升高没事。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有几个问题请教下
1.规格书上说,bq25895最大充电电流可以到5A, 这有没有特定的输入电压要求。我在外部稳压源输入10V以上时可以达到5A的充电电流,但输入电压为5V时,达不到5A
2.如何让快充输出不同的电流,我买了华为的充电器SuperCharge 支持5V/2A,4.5V/5A,5V/4.5A ,但使用时只能输出5V/2A,是否895不支持这个充电器
3.用外部稳压源输入,当逐渐调低电压的时候,895会停止充电。电压升高没事。
Hi
输入的限流电是3.25A, 而topy上是降压,电池充电是5A时,假设此时buck的输出是4V, 效率是90%,输入电流为3A, 那么4V*5A/90%/3=7.4V, 所以并非所有电压范围内都能维持5A充电。如果你的效率达不到,并且电池电压较高导致buck输出较高,则需要更高的输入电压。
如上,当输入电压较低时,电池充电电流也就较小了。在可充电范围内电流可通过寄存器设置。