This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq28z610 循环学习

Other Parts Discussed in Thread: BQ28Z610, BQSTUDIO, BQPRODUCTION

1. 根据实际项目规格配置DF参数,选择正确的CHAM ID烧入.

2. 对板子进行校正。

3. 导出这个时候的senc文件备用。

4. 连接电芯到板子,发送reset命令,得到Golden Pack.

5.   把电池放空到3.0V,然后静置5个小时。

6. 发送0X21命令使能IT算法。

7. 把电池充到饱,确保有效的充电中止(100%,FC置位),然后停止充电。

8. 静置两个小时。

9. 把电池以C/5放空到终止电压,然后停止放电。

10. 静置5个小时。

11.  重复7~10步骤一次

       对于bq27510:当update status的数值为0x02,Ra flag是0x0055时,说明学习成功。

12.导出gg文件,手动修改cycle count=0, lifetime etc;

13. 烧入第3步备份的senc文件。

14. 导入第12步修改好的文件, 得到golden sample.

15. 从BQSTUDIO里面生成量产文件。

以上步骤:第3步是必须要有的吗?一块板子循环学习完成后再导出senc文件和gg文件可否?