This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

双向DC-DC隔离电源 用于电池的均衡



您好!

        请问贵公司有没有做双向DC-DC隔离电源的控制芯片呢?我的设计要求如下

Input:1.6V-2.5V   Output: 5V   DC-DC升压模式均衡持续电流不低于15A,降压

模式不低于20A

降压模式效率>88%

升压模式效率>83%

希望能给出相关的资料谢谢!