您好!
请问贵公司有没有做双向DC-DC隔离电源的控制芯片呢?我的设计要求如下
Input:1.6V-2.5V Output: 5V DC-DC升压模式均衡持续电流不低于15A,降压
模式不低于20A
降压模式效率>88%
升压模式效率>83%
希望能给出相关的资料谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.