Other Parts Discussed in Thread: TPS54231, TPS54620
我在做一个24V转5V的DC/DC,电路搭建后调试正常,然而在做负载短路实验时,发现这么一个问题:输出我用短路线短路(短路可靠,我用焊接的方式把5V短路),24V输入的电流(A1)是0.17A,5V输出的电流(A2)是2.93A,然后测了TPS54231的8脚(PH),看到一个频率是66.7KHZ的波形,占空比是5%,我想问下,这是怎么回事?按照道理,短路了,芯片应该关闭输出或者是打嗝,但是就算是打嗝,66.7KHZ的频率是否太高了,输出电流接近3A,如果长期短路,那势必会损坏TPS54231,不知道TI的工程师能否帮我解决这个问题,谢谢!